I am testing an SN74LVT244DBW using a Hutron Model 32, which is a the military version of the 3200S. When probing any input pin (in relation to ground) I get what appears to be distortion starting at about 12V. That is, the signature produces random, unstable current levels where the base signature is 0V and no current. I liken it to the crackling distortion you might hear when you overdrive your speakers. I know the answer is to not test these above 12 volts, but I was hoping some engineer could comment on this. The test signals are 15V, 10K ohms and 200 Hz and 20V, 50K ohms and 200Hz.
Thanks!
Brian Fowler
NUWC DET FEO NORFOLK