Other Parts Discussed in Thread: HD3SS460
Hi,
I'm testing HDMI output on USB-CTM-MINIDK-EVM board, but it doesn't work.
The other functions of the board work perfectly.
The host side is a Galaxy Tab S6 which has ALT mode, and it surely works with other TypeC-to-DP modules.
Sound is also not working.
When the type C cable is connected between the Galaxy Tab S6 and the board, the sound of the Galax Tab S6 goes mute, just as an external sound device was connected.
But, I cannot listen anything from the 3.5mm pi jack on the board.
All the result are the same when I connect 20V source to the DC jack.
Do I have to config something before I use it?
Below is the connection status.