Part Number: DP83TD510E-EVM
Other Parts Discussed in Thread: USB-2-MDIO
Development board DP83TD510E-EVM (two devices, two WIN7/WIN10 PC) is not recognized when connected via USB. All jumper settings are default. What is the problem?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DP83TD510E-EVM
Other Parts Discussed in Thread: USB-2-MDIO
Development board DP83TD510E-EVM (two devices, two WIN7/WIN10 PC) is not recognized when connected via USB. All jumper settings are default. What is the problem?
Please try replacing R24 with 0ohms (connected to USB) to access the USB port.
--
Regards,
Vikram
Thank you for advice! Provided solution did help. Development board was recognized as MSP430-USB Examaple VID_2047 PID_0300.
The next problem is that the "standalone drivers pack" that was provided in manual (there was a link to download site) does not contain drivers for such device. Maybe they are contained in full development tools pack from TI?
Hello Igors,
Which driver pack are you referrring to? Can you please point me to the manual section?
--
Regards,
Vikram
DP83TD510E-EVM User’s Guide:
----------
4.1 MSP430 Driver Install the latest MSP430 driver from this website: software-dl.ti.com/.../ msp430/MSP430_FET_Drivers/latest/index_FDS.html http://software-dl.ti.com/msp430/msp430_public_sw/mcu/msp430/MSP430_FET_Drivers/latest/index_FDS.html
------------
But this set does not contain the necessary drivers :(
Hello Igors,
I see that the site is down at this moment. But I could see MSP drivers on this site yesterday. May be you can share the driver you have downloaded from the site and I can confirm if the driver is ok or not.
Archive content:
Directory of C:\ti\fetdrivers
21-Apr-21 19:48 <DIR> .
21-Apr-21 19:48 <DIR> ..
21-Apr-21 19:48 0 b
16-Apr-21 12:19 <DIR> emulation
16-Apr-21 12:19 <DIR> install_logs
13-May-19 12:27 160,544 MSP430_USB_Drivers_Software Manifest_WIN.pdf
16-Apr-21 20:43 <DIR> uninstallers
2 File(s) 160,544 bytes
Directory of C:\ti\fetdrivers\emulation
16-Apr-21 12:19 <DIR> .
16-Apr-21 12:19 <DIR> ..
16-Apr-21 12:19 <DIR> drivers
0 File(s) 0 bytes
Directory of C:\ti\fetdrivers\emulation\drivers
16-Apr-21 12:19 <DIR> .
16-Apr-21 12:19 <DIR> ..
16-Apr-21 12:19 <DIR> msp430
0 File(s) 0 bytes
Directory of C:\ti\fetdrivers\emulation\drivers\msp430
16-Apr-21 12:19 <DIR> .
16-Apr-21 12:19 <DIR> ..
16-Apr-21 12:19 <DIR> DPInst
16-Apr-21 12:19 <DIR> USB_CDC
16-Apr-21 12:19 <DIR> USB_eZ-RF
16-Apr-21 12:19 <DIR> USB_FET_Win7_8_10_64
0 File(s) 0 bytes
Directory of C:\ti\fetdrivers\emulation\drivers\msp430\DPInst
16-Apr-21 12:19 <DIR> .
16-Apr-21 12:19 <DIR> ..
13-May-19 12:27 552,528 DPInst.exe
13-May-19 12:27 1,047,632 DPInst64.exe
2 File(s) 1,600,160 bytes
Directory of C:\ti\fetdrivers\emulation\drivers\msp430\USB_CDC
16-Apr-21 12:19 <DIR> .
16-Apr-21 12:19 <DIR> ..
13-May-19 12:27 59 installCerts.bat
13-May-19 12:27 17,842 msp430tools.cat
13-May-19 12:27 4,019 msp430tools.inf
13-May-19 12:27 4,245 USB_CDC_CERT.p7b
4 File(s) 26,165 bytes
Directory of C:\ti\fetdrivers\emulation\drivers\msp430\USB_eZ-RF
16-Apr-21 12:19 <DIR> .
16-Apr-21 12:19 <DIR> ..
13-May-19 12:27 17,151 430cdc.cat
13-May-19 12:27 2,822 430CDC.inf
13-May-19 12:27 56 installCerts.bat
13-May-19 12:27 4,245 USB_eZ_RF.p7b
4 File(s) 24,274 bytes
Directory of C:\ti\fetdrivers\emulation\drivers\msp430\USB_FET_Win7_8_10_64
16-Apr-21 12:19 <DIR> .
16-Apr-21 12:19 <DIR> ..
13-May-19 12:27 525,792 difxapi.dll
13-May-19 12:27 8,637 ump3410.cat
13-May-19 12:27 14,336 umpf3410.i51
13-May-19 12:27 56,320 umpusbvista.sys
13-May-19 12:27 5,276 usbuart3410.inf
13-May-19 12:27 1,721,576 WdfCoInstaller01009.dll
6 File(s) 2,331,937 bytes
Directory of C:\ti\fetdrivers\install_logs
16-Apr-21 12:19 <DIR> .
16-Apr-21 12:19 <DIR> ..
16-Apr-21 20:43 9,172 ti_msp430driver_setup_1.0.1.1_install.log
1 File(s) 9,172 bytes
Directory of C:\ti\fetdrivers\uninstallers
16-Apr-21 20:43 <DIR> .
16-Apr-21 20:43 <DIR> ..
16-Apr-21 20:43 5,764 ti_msp430driver_setup_1.0.1.1.dat
16-Apr-21 20:43 6,323,203 ti_msp430driver_setup_1.0.1.1.exe
2 File(s) 6,328,967 bytes
Is the issue resolved? Did you try using usb-2-mdio tool to read/write register? I checked and EVM should have pre-flashed MSP430 code and you should be able to read write register using usb-2-mdio tool. If for some reason, MSP is not responding then you can flash the attached by following the user guide.msp430-usb2mdio-firmware-2.7.txt