Part Number: TUSB8042
Hello Team,
we are planning to use the TUSB8042 on a board but some pins will not be used.
Can you confirm the understanding below?
unused USB_SS_TX output pins can be left floating.
The datasheet says:
When the upstream port is connected to an electrical environment that only supports
full-speed/low-speed connections, SusperSpeed USB and high-speed connectivity
are disabled on the downstream ports.
So, I am guessing that the unused USB_SS_RX inputs pins can also be left floating.
Is this correct?
While we don’t need power from upstream, I suppose we will still connect
the voltage divider to USB_VBUS monitor input.
Special requirements for the voltage power sequencing?
Thanks,
SunSet