Part Number: MAX3232
Hello,
i´m working on a simple ESP8266 and MAX3232CPWR design.
I´m experiencing following issue at the input side of the MAX3232 IC:
- when the ESP Micro is connected to the MAX, RX signal voltage level is ~ 1.5V (below the treshhold of the IC), TX pin works fine signal level is here at the expected 3.3V
- ESP not connected to the MAX has a perfect output of the signals
Behaviour looks like some voltage divider / pull up inside the ic?
Could someone point me towards the exact issue?
Below are details for this issue.
Thanks in advance!
Following actions have been done:
- changed MAX chip to avoid defect part -- no change
-checked resistance between RX and TX and each line to GND and the sourunding components. No observations found.

Osci shot of signal overview, both have the same V/div setting.

detailed view on the RX signal, measured signal amplitude is 1.5V.

ESP output without the MAX3232 Connected

Routing

Schematic