Part Number: TUSB4041I
Dear team
My customer would like to use the TUSB4041I, but have some confuse about the applications.
1. Is there a reference design with this HUB can be used as evaluation?
2. if customer just use the default use case, 1 in 4 out HUB, by default register setting, will our device working under standalone mode without I/C//EEPROM?
3. How to use the OTP mode?
4. If using the default mode, will the hub compatible with standard driver and OS?
Thanks
Jun Shen