Part Number: DS90UB914A-Q1
Hi all,
I got a question about FPD-Link III. My customer would like to use a STQ cable to supply power and transmit data at 913A-914A. Can you tell me if the configuration inside STQ cable below possible?
- Cable 1: Connection between DOUT+ of 913A and RIN0+ of 914A
- Cable 2: Connection between DOUT- of 913A and RIN0- of 914A
- Cable 3: GND for power
- Cable 4: +7V/1A_max for camera. This voltage is created by a DCDC converter with fsw=2.2MHz.
STQ cable itself can pass the insertion loss spec of FPD-Link III requirements. If there are any concerns or things to consider, please let me know.
Regards,
RYO