Part Number: DS90UB960-Q1
Hello TI team,
By default a CSI2 camera sensor will be connected to the ECU. Sensor Spec and CSI2 spec has been given below.
Camera sensor:imx327lqr-c
1920*1080 Resolution, Progressive scanning
RAW 10 Image format
30 fps
CSI2 Spec:-
CSI2 V1.3- Raw10,
Four Lanes,
1162.5Mbps per lane,
111.375 MHz CLK
I would like to replace this camera and source the images at 30fps from my industrial PC. My industrial PC comes with 953 Serialiser and has Fakra connector. I am planning to use 960Q1-EVM as deserialiser.
1. Can 960Q1 replace the camera with aforementioned spec ?
2. Do i need to connect the supply voltage from ECU (3.3V) to 960Q1 deserialiser. ?
3. Any additional circuit for PoC to be done ?
4. Do i need to consider any signals apart from the Pin Mapping shown below ?