Part Number: DS90UB913A-Q1
Hi, Team,
I can't find the AC Electrical Characteristics for the 913,914's GPIOs in datasheet. Can these GPIO support the PWM's output? How about the limitation for the PWM input/output?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB913A-Q1
Hi, Team,
I can't find the AC Electrical Characteristics for the 913,914's GPIOs in datasheet. Can these GPIO support the PWM's output? How about the limitation for the PWM input/output?
Hello Wu,
which OWM frequency are you looking for?
We have not validated the min or max specs for PWM. So, if you tell me the frequency and the duty cycle of your signal, I can tell you if this is supported or not.
Customer need 2 PWM, the frequency are 60Hz / 30kHz, duty cycle is 0 ~ 100%. If the duty can't meet the spec, pls give the recommended duty range.
30KHz is not possible. You can send max 20KHz over the back channel.
Duty cycle is possible from 0% to 100%
Hi, Hamzeh,
How about 90UB935/936 and 90UB953/954? Can they support the same PWM spec? Thanks!