Part Number: TUSB4041I
Hi,
I have few questions about TUSB4041I this part:
1. What does personal power control mean? What is the difference between the two?
0 = Individual power control supported when power switching is enabled
1 = Power control gangs supported when power switching is enabled
2. Port 1 and port 4 add USB current limit, Port 2 and Port 3 have no USB current limit, then should I set FUllPWRMGMTz this pin to be high or low?
3. If there is no need to have USB battery charging, then PWRON1_BATEN1/ PWRON2_BATEN2/ PWRON3_BATEN3/ PWRON4_BATEN4 should set to low. Is that correct?
Thanks.