Part Number: MAX3243E
Hi Team,
Attachedis the schematic diagram of the MAX3243E.
When power vcc=3.3V ,And com2,com3,com4 are connected to three devices at the same time, all the devices will be unable to use,
There is no problem in connecting any two devices.
When power vcc=5V, the three devices can work normal.
Is it possible connected to three devices and the supply voltag is 3.3v?
Can you help solve it?
Thanks and best regards