Part Number: TCAN334G
I have a system deployed with a customer that uses TCAN334Gs for all nodes in the bus. They had an incident where 32V was shorted somewhere it shouldn't and not-surprisingly a number of the TCAN334Gs failed, but not all of them. They continued operating the system after replacing the not-working 334Gs. Despite no obvious problems from that point in terms of ESD or DC voltage problems, a number of the transceivers that survived the initial event failed, and new transceivers that were on the bus with them failed too. All of the failures manifest as low resistance paths between one of CANL or CANH to ground or VCC.
I have two questions:
1. How likely is a transceiver to fail days or weeks after an over-voltage event?
2. Is there any plausible mechanism whereby such a delayed failure could cause other new transceivers on the bus to also fail?
This particular customer doesn't believe that they have had any user initiated problems since that first transient, but we are trying to figure out if there are actually ongoing ESD or other problems, or if we instead need to simultaneously replace all transceivers in the system.
In this case there are 4 buses, each with 4 nodes. Each bus is approximately 0.5m long. This particular customer only has one end of each bus terminated. There are no ESD protection diodes on the CAN lines, although in this application, other than incidents with high DC voltages being applied to the CAN lines, no failures have been observed in several hundred deployments.
Thanks!