Part Number: DS90UB936-Q1
Hi Team,
In section 7.5.9 of the 936 datasheet, the section reads "When the DS90UB936-Q1 detects an error condition the standard operation would be to flag this error condition and truncate sending the CSI-2 frame to avoid sending corrupted data downstream. When the DS90UB936-Q1 recovers from an error condition, it will provide Start of Frame and resume sending valid data."
However, the default settings in register 0x7C and 0x7D do not take any action if an error is detected, a user would need to set those. So when the above statement refers to "standard" operation, that is meaning that a user should go in and a change the registers in 0x7C and 0x7D to meet "standard" operation, correct?
Thank you,
Jared