Hi Experts,
Can 925 - 926 support below video stream?
- LVDS 8 bit,
- R. G. B. Strip
- 1280 x 800 @ 60Hz
- 16.7M colors
Piotr
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Experts,
Can 925 - 926 support below video stream?
Piotr
Hello Piotr,
Thanks for reaching out.
Re: “• LVDS 8 bit, ”
925 and 926 devices support LVCMOS inputs. But, it looks you are looking for an LVDS solution. A better fit would be DS90UB927-Q1 and DS90UB928-Q1 from our portfolio.
Re: “• 1280 x 800 @ 60Hz”
We are not sure about your timing spec.
But, if we assume your video timing spec matches the standard video timing for 1280 x 800 display panel, then the following are applicable:
Visible area = 1280, Front porch = 64, Sync pulse = 136, Back porch = 200, Whole line = 1680 pixels
Visible area = 800, Front porch = 1, Sync pulse=3, Back porch=24, Whole frame = 828 lines
We can use the following equations to determine:
From this we can conclude that the PCLK rate is within the allowed range (5-85MHz) for DS90UB927-Q1 and DS90UB928-Q1.
Please let us know if your timing spec is different from above assumption so that the PCLK rate can be calculated correctly.
Regards,
Solomon