This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN4550: TCAN4550 can support 5V system?

Part Number: TCAN4550

TCAN4550 can support 5V system?

  • Hi Kevin,

    Yes, TCAN4550 is designed to work on a CAN bus with other 5V CAN transceivers that meet the ISO 11898-2 specification. The device itself requires a Vsup supply between 5.5V and 24V for proper operation. 

    Let me know if you have any more questions.

    Regards,
    Eric Schott