Other Parts Discussed in Thread: DP83867IR
When connecting 100BASE-TX to each other on the board, I think that a transformer is not required and it is sufficient to connect directly, but is it correct?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: DP83867IR
When connecting 100BASE-TX to each other on the board, I think that a transformer is not required and it is sufficient to connect directly, but is it correct?
Thank you.
It has a configuration similar to VME and connects CPU boards with 100BASE-TX.(Only inside Subrack)
The board will be newly designed including the back board.
Device Candidates>
PHY: DP83867IR
L2SW: KSZ8795CLX
Connection image>
| CPU board | Backboard |
1: MAC(CPU)-PHY-Connector-L2SW
2: MAC(CPU)-PHY-Connector-L2SW
3: MAC(CPU)-PHY-Connector-L2SW
4: MAC(CPU)-PHY-Connector-L2SW
5: MAC(CPU)-PHY-Connector-L2SW
Hi Masaru,
I would recommend that you refer to this for app note for ethernet without a transformer.
https://www.ti.com/lit/an/snla088a/snla088a.pdf
I also recommend that you review specific device datasheet for MDI implementation.
Kind Regards,
Joe
All information in this correspondence and in any related correspondence is provided “as is” and “with all faults”, and is subject to TI’s Important Notice (http://www.ti.com/corp/docs/legal/important-notice.shtml)