Part Number: DS90UH941AS-Q1
Hi team,
I have below questions, could you please help give comments?
1. My customer use FPDLINK III by a HSD connector with a total of 4 signal wires for LVDS0+/- and LVDS1+/-.
Now they want to connect the power cable from this HSD connector .
So can the power cable for 12V@2A route on the LVDS0+/- ?
2. Does the 941 have the ability to flip the image output from the DSI?
The customer has rotated 180 degrees on the screen design, so they want to know if it is possible to rotate the image 180 degrees through the FPD-LINK.
Thank you!
Ivy