Part Number: TUSB216
Other Parts Discussed in Thread: TUSB214,
Hi, Support Team
A customer is developing a product using the TUSB214.
Currently, TUSB214 is being used by utilizing I2C Control.
For DC BOOST setting, I2C Register is being used in Disable status as shown below.

Please confirm the inquiries below.
1. Is the TUSB214 and TUSB216 100% compatible in hardware?
2. Is the TUSB214 and TUSB216 100% compatible with software?
-Whether the I2C Address is the same (It appears to be the same when comparing datasheets.)
-Setting register such as AC Boost and DC Boost setting, setting stage, level is the same
-Can TUSB216 disable DC Boost through I2C like TUSB214?
3. Based on TUSB216, Pin No. 11 is CDP_ENZ (CDP Enable), and when it is low, CDP operation is shown. What does it do if it is in a floating state?
Thanks.
Regards,
MJ