Part Number: DP83869HM
Hello,
I've a board with a DP83869HM Ethernet PHY.
All is OK in unicast or broadcast operations: ARP commands, UDP messages [...] are received/transmitted correctly...
I should receive a video camera stream in a multicast way (IP address in 239.x.x.x, MAC address with 40th bit at 1). The manufacturer of that camera says me that there is no special negotiation to follow between their camera and my board (no subscription packet or such things: the camera streams as soon as it is powered).
Do you know if there is some special register configuration to perform in the Ethernet PHY so as to receive multicast packets? I don't see any such registers but maybe I've missed something.
Do you have any idea of the non-reception of video packets?
Many thanks,
AD.