Part Number: DS90UB960-Q1
Hi Team,
In the 960 datasheet, I see equation 2 for the output BW of Best-Effort Round Robin, Basic Synchronized, and Line-Interleaved CSI-2 forwarding. If I am using four cameras that a different resolutions, how should I consider this equation? Should I take an average of all four camera's Hactive and Nbits/pixl? Or should I select the largest Hactive parameter and largest Nbits/pxl from the imager options?
As an example, let's say I have the following four camera specs:
Sensor 1: Hactive = 1080, Nbits/pxl = 12
Sensor 2: Hactive = 1280, Nbits/pxl = 12
Sensor 3: Hactive = 720, Nbits/pxl = 18
Sensor 4: Hactive = 720, Nbits/pxl = 24
Thank you,
Jared