This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS125DF111: DS125DF111 Technical problems

Part Number: DS125DF111
Other Parts Discussed in Thread: DS280DF810, USB2ANY, DS280BR810

Hi team,

My questions are as follows:

1. is there a reference design under the control of MCU?

2. Under the control of MCU, is it master mode or slave mode?

3. In the case of MCU control, whether add0 / ADD1 is needed, my design is to use a MCU to control a ds125df111

4. is there Diagram of clock and data, and the command, read / write, address, etc. in the datasheet can be indicated?

Best regards,