Part Number: TUSB7320
Let me ask you a question about TUSB7320.
Is there a register to change the PHY Boost (EYE pattern) on the USB line side of the TUSB7320?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TUSB7320
Let me ask you a question about TUSB7320.
Is there a register to change the PHY Boost (EYE pattern) on the USB line side of the TUSB7320?
you can boost eye pattern by changing Swing with external EEPROM (0Eh to 11h). Pls see section 7.4.1.3 in datasheet
Thank you for your reply.
I have two questions.
1) Is the boost eye pattern accessible from PCI registers?
2) Is it possible to set the boost eye pattern with USB 2.0 (terminal name: USB_DM_DN2, USB_DP_DN2)?
1: from eeprom register, not PCI register.
2: sorry, boost eye can not do for USB2 from register, you can lower external resistor between R1EXT and R1EXTRTN to boost USB2 eye.
Thank you for your reply.
SLLSE76M –MARCH 2011–REVISED JULY 2015 19 page
SERIAL EEPROM WORD ADDRESS:0Eh
BYTE DESCRIPTION:PCI E4h, De-emphasis and Swing Control, Byte 0
In 1), you answered that it is not a PCI register, but there is a description of the PCI register address in the above description, but is it different?