Part Number: TPS66120
In the page 17 from the datasheet SLVSEW9B–AUGUST2019–REVISEDDECEMBER2019 there are some descriptions of the conditions to change of status. The first 2 conditions seem to change from the pin EN1. I cannot find EN1 pin, only EN0. Also the EN1 only apears in this page in the full document. Could this be a typo error? Or is there a EN1 pin to connect?