Part Number: LMH1297
Greetings,
I have a card with 4 LMH1297s on it. Each channel is exclusively an Input or an Output, so SDI_OUT is not used. There is some performance degradation when I run a TX adjacent to an RX through a long channel (approx -40db), and I'm looking to improve the next spin of the design to minimize the degradation. Would it be beneficial to separate VIN and VDD_CDR onto different planes which I tied together a common point somewhere else on the board? Our current design has these pins sharing the same 2.5V plane, which is isolated from the other LMH1297s through ferrite filters. The EVB has these supplies on separate planes which are tied together at a header.
Thanks