Part Number: TLK1501EVM
Other Parts Discussed in Thread: TLK1501
Hi,
Good day.
Our customer has a question regarding the TLK1501EVM. Kindly see below.
""I have a doubt about the use of the 10nF capacitor connected to ground between the two 50ohm termination resistors on the evaluation board of the TLK1501 (RX lines)
On the datasheet there is no capacitor between the termination resistors, and the line is described as differential terminated with 100ohm in total, while on the evaluation board there is the 10nF capacitor which seems showing the RX lines as two single ended 50ohm lines.
Could you please let me know if the 10nF capacitor is required, and what is its use?""
Looking forward to your inputs. Thank you.
Regards,
Cedrick