Part Number: DS90UB949-Q1
To address existing part shortages, can the DS90UB949 be used in place of a DS90UB929? Same question for the DS90UH949 in place of a DS90UH929?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB949-Q1
To address existing part shortages, can the DS90UB949 be used in place of a DS90UB929? Same question for the DS90UH949 in place of a DS90UH929?
Hello David,
The difference between 929 and 949 is that 929 supports single FPD-Link only, while 949 can support either single or dual link. So yes, 949 can be used in place of 929, but for the other way around, you would need to verify that the video link can fit the bandwidth of single FPD-Link if the system was previously using dual.
Best Regards,
Casey
HI Casey;
Thank you for the prompt reply. Would there be any SW or register differences, or could the '949 just drop into the existing '929 application?