Part Number: SN65DPHY440SS
Hello,our client is using 10.1-inch sub screen (800 * 1280) which has a Mipi (DSI) interface, the distance between the main board and the LCD MIP interface of the sub screen is 350mm-400mm (through twisted pair + PCB wiring + FPC, 100 Ω± 10 impedance);
Now, considering that the Mipi line is too long (standard 150 mm), SN65DPHY440SS is selected for Mipi extension;
Please help evaluate the following questions:
1. How long can SN65DPHY440SS extend the Mipi signal? Is 350mm feasible?
2. Mainboard uses LT9211 (Longxun,used for converting DPI to Mipi). Please evaluate whether LT9211 can be used with sn65dphy440ss?