Part Number: TPS65988DJ
Other Parts Discussed in Thread: TPS65988DK
hi,
Below is the spec. from a local customer. the project is similar with a docking. would you like kindly help check if TPS65988DJ can support those requirements?
Type-C PD controller requirements are as follow:
1.Support USB Power Delivery (USB-PD) 3.0
2.Support Two integrated USB-PD Type-C ports
3.Support UFP[1] (RD) and current sources for DFP[2] (RP) on both Type-C ports
4.Support overvoltage protection (OVP) and overcurrent protection (OCP) on the VBUS
5.Support detect voltage and current on the VBUS
6.Support sleep mode
7.Support fast role swap
8.Support gate drivers for external VBUS PFET control on Type-C Ports
9.More than 14 GPIOs
10.More than 10 channel ADCs
11.CC line signal can wake up PD controller