This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25750: Battery level indicator with TPS25750 and BQ25792

Part Number: TPS25750
Other Parts Discussed in Thread: TIDA-050047,

Is it possible to use the ADC and GPIOs on the TPS25750D to drive a battery level quad LED indicator, as per the block diagram? 

E.g. for a 4S Li-Ion battery, 

100% 4 LEDs on

75% 3 LEDs on

50% 2 LEDs on

25% 1 LED on

I am using the TIDA-050047 reference design with the TPS25750D and the BQ25792 charger IC.

Thanks

Tony