Part Number: DP83867IR
Other Parts Discussed in Thread: DP83867ERGZ-R-EVM
Hi There,
I use "DP83867IRRGZR".
I have some questions on the evaluation board.
Evaluation Board
Project Title:DP83867ERGZ-R-EVM
File:SV601189A_DP83867ERGZ.SchDoc
1. RX_DV / RX_CTRL is DNP for R21 and R23.
RX_DV / RX_CTRL sets auto-negotiation.
Auto-negotiation is valid only in mode 3 or mode 4.
Why is mode 1 set on the evaluation board?
2. There is a note below.
CFG4 [7] is RESERVED, is it correct?
>If the RX_CTRL pin cannot be strapped to mode 3 or mode 4, bit[7] of Configuration Register 4 (address 0x0031) must be cleared to 0.
Best regards
- satoshi