Part Number: DS90UB954-Q1
Hello Team,
I got a question from customer about FPD3_MODE selection.
Q. Datasheet says "Each input port can be individually configured for CSI-2 or RAW modes of operation". Does it mean that we can set CSI-2 mode for port0(RIN0+ and RIN0-), RAW mode for port1(RIN1+ and RIN1-)? If so can you please let me know how to set like this?
Q. Datasheet says "The input mode of operation is controlled by the FPD3_MODE (Register 0x6D[1:0]) setting in the Port Configuration register. The input mode may also be controlled by the MODE strap pin." If the MODE pin voltage set RAW10, and register 0x6D[1:0] set CSI mode, which setting is prioritized?
Thanks,
Yuta Kurimoto