Part Number: TVS3301
Other Parts Discussed in Thread: TVS3300,
Hi,
Can you suggest me an alternate for this
The standoff needs to be same
the max voltage should be 40V
should pass IEC 61000-4-5 (8/20 µs) at 500V 250A
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sahil,
Unfortunately, this is the only 33 V Vrwm part we currently have besides the unidirectional version, TVS3300. TVS3300 has a slightly higher IEC 61000-4-5 rating of 35 A, but unfortunately it is not close enough to your requirement of 250 A.
Regards,
Matt Smith
Hi Matt,
Thanks for your reply.
Does TI has a TVS according to my requirement
33V standoff and 40V max clamping voltage
The IEC 6100-4-5 requirement remains the same
Hi Sahil,
No, we do not. The TVS3300 and TVS3301 meet the 33 V standoff voltage and 40 V max clamping voltage requirement, but not the 250 A IEC 61000-4-5 requirement.
Regards,
Matt Smith