Other Parts Discussed in Thread: TUSB9261, TUSB9261DEMO, TUSB9260
I am using the TUSB9261 Flash Burner with the TUSB9261 Demonstration & Reference Design TUSB9261DEMO.
When I start the Flash Burner no devices are shown in the device tree of the burner.
In the XP Device Manager the TUSB9261 appears as:
Figure 2-7. TUSB9260/TUSB9261 Instances With FW Containing Mass Storage Instance Only (No HID)
If I remove the SPI Jumper and reset the board it appears in the tree.
I replace the jumper and reset the board it is gone.
I reprogrammed the board with the latest firmware:
TI TUSB926x Default Firmware, U1_U2 Disabled (Rev. I) sllc416i.zip
and see the same behavior.
Why doesn't the device appear when the jumper is installed?
Thanks - Don