Other Parts Discussed in Thread: TS3DV642,
Dear Sir,
TS3DV642 and HD3SS215 are 2:1/1:2 Differential Switch
How to choose?
HD3SS215 are there any function better than TS3DV642?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Vincet,
This is a summary of the main differences between HD3SS215 and TS3DV642.
|
Part # |
HD3SS215 |
TS3DV642 |
|
# of Pins/Balls |
50/56 |
42 pin |
|
Package Size |
5mm x 5mm |
9mm x 3.5mm |
|
-3dB bandwidth |
7 GHz |
PortA 6.9 GHz PortB 7.5 GHz |
|
Dynamic Char Freq* |
3GHz |
1.7GHz |
|
Cross Talk (dB) |
ZQE -35dB RTQ -35dB |
-40 dB |
|
Isolation (dB) |
ZQE -22dB RTQ -16dB |
-23 dB |
|
Insertion Loss (dB) |
ZQE -1.6dB RTQ -2.4dB |
PortA -0.75 dB PortB -1.0 dB |
|
Return Loss (dB) |
ZQE -12dB RTQ -13dB |
-15.9 dB |
|
Power (Active) |
<9mW typ |
180uW typ |
|
Power (Low) |
< 30uW typ |
< 30uW typ |
|
VCC |
3.3V |
2.6V to 4.5V |
|
ESD (HBM) |
1.5kV |
2kV |
|
Temp Range (˚C) |
0 to 70 & -40 to 85 |
-40 to 85 |
Regards