This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi.
I use a DP83848w with stm32f107. ARM program and PHY work successfully for first time and I got my socket connection on Hyper-terminal, but the link led turned off when I reseted the board for debugging and it never be turn on !
I cant find any issue on software after many reset and analyze the PHY register.
BMCR is 0x3100 & BMSR is 0x7849 -> no linking
I turned off the board and turned it on again after 30 min.(I worked on other things.) Its OK again! but when I reseted, no linking available.
I tested :
1- 10M half duplex, no link.
2- loop-back cable,no link.(loop-back cable tested before with a Ethernet switch and led of switch turned on)
Its seems that my PHY cant negotiate or create active link for a reason.
whats the problem(s) ?
Thanks.
Please send your schematics to me at (email address redacted). I will review them to see if there are any items of concern.
Please also post the complete register contents (register addresses 0x00 - 0x1F). Some of the device registers latch low or high to capture status so please read each register twice before providing the register contents.
What partners are you testing with? What are the other PHYs for which a link is not re-established?
Patrick
Thats I forget to say that, Connection is RMII.
Register Contents are:
Address-Value
0x00-0x3100
0x01-0x7849
0x02-0x2000
0x03-0x5c90
0x04-0x01E1
0x05-0x0000
0x06-0x0005
0x07-0x2001
0x08-0x0000
//---------
0x10-0x0000
0x11-0x0000
0x12-0x0000
0x13-0x0000
0x14-0x0000
0x15-0x0000
0x16-0x0100
0x17-0x0021
0x18-0x0000
0x19-0x8021
0x1A-0x0904
0x1B-0x0000
0x1C-0x0000
0x1D-0x6011
0x1E-0x003F
---------------------
This schematic is not important design and I put schematic here (may be used for other one):
also available on this.
I tested with my PC(Realtek PCIe GBE Family Controller->RTL8167) and a D-link unmanaged switch(DES-1008D).both response are same.
Thanks in advance.
I checked register again without any good news.
I checked ST source code example and board response was same and no led turned on. thats seems hardware has a issue.
schematics available on previous post.
please continue your helping.
Thanks.
Hello,
Have you measured the voltage on the RBias resistor?
Can you check the 50MHz clock source and confirm frequency?
Thanks,
John
Yes.
50MHz signal is OK (approximately sinusoidal waveform).
RBias is 1.185Vdc. (I don't know true values.)
Are the registers contents OK?
Thanks.
I do not see any issues with the register configuration. The schematic connections look correct. The RBIAS voltage should be ~1.2V so the value of 1.185V is reasonable.
I have a few more recommended measurements to try:
If all these values appear correct, we can evaluate the transmit signaling at the RJ-45 connector and we can run some tests with internal and external loopback (using a loopback cable) to help narrow down the source of the trouble.
Patrick
I can work on this board again and changed DP83848 with new one and everything were same as ago.
I checked your test solution:
1. 3.3 is OK
2. PF voltages are 1.71v
3.a) Rbias is 4.81K .
3.b)resistance between transmit and receive can not measurable because Rj45 connector change true values. but when I checked the board I see these are 68X (49.9Ohm). measured values are ~0.6Ohm(resistors are parallel with RJ45 Trans).
I cant fix this problem yet. whats the next step?
Thanks.
I set Loopback flag. Green LED turned on and link flag changed to 1.
Its not useful because real network has problem and I cant check my software well.
I checked everything and I changed RJ45 Connector with new one at-last.
everything is OK now and link is available. Its seems damaged by high temperature soldering,Its not my work :) .
Its a bad problem and may be a ridicule. but I never think that is problem.after all,I learned new thing about this chip.
Thanks for helping.
Happy Christmas and Have a good year.
Thank you for providing this feedback. I would suggest that this is a not a very common source of communication problems. I commend you for your diligence in working through all the possibilities and driving this to a successful conclusion.
Patrick