This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About Fail safe of AM26LV32E

Guru 19685 points

Other Parts Discussed in Thread: AM26LV32E, AM26LV32, TINA-TI

Please let me know below about Fail safe of AM26LV32E.

The Fail-safe circuit of AM26LV32E is considered to be the following.

VA-VB=[3.3/(200k+5k+200k+5k+221)]×(5k+5K+221) ≒80mV

 

VA-VB=[3.3/(200k+5k+200k+5k)]×(5k+5K) ≒80mV

 

In the upper calculation, I think that VID=200mV is not securable.

Is my calculation method wrong?

Moreover, do intend to terminated=OPEN?

 

Best regards,

Satoshi

  • Satoshi-san,

    You calculation is correct. There is just 80mV at VA-VB and the VID at port pins can be zero volts.
    Yet the device has shorted input fail safe. Therefore the AM26LV32E  is designed and tested such that a VID of 0V results in a output high. That means both VIT+ and VIT- are negative voltage in the range -0.2V to -0V.

  • Dear Ron Michallick-san

    Thank you for reply.

    Is AM26LV32 classified into Transceiver"Z" of the attachment application note?

    1033.slyt514.pdf

    Consequently, Is VID<=200mV have no problem for the fail-safe of AM26LV32?

    Moreover, is fail-safe only short?
    (Doesn't it correspond to Open?)

    Best regards,

    Satoshi

  • Satoshi-san,

    Yes it is like Transceiver "Z". Fail safe for short (port A to B); fail safe for Open (port A and Port B no connection); and Terminated (port A and B only connected to line termination resistor).

    Pages 7 through 11 in data sheet have cautions to make sure the fail safe works correctly. 

  • Dear Ron Michallick-san

    Thank you for the advice.

    Please let me also know the following by addition.

    This time, the client will replace to AM26LV32 at RS-422.

    Since the RS-422 device which was being used in the past had not carried out Fail-Safe correspondence, it constituted from external resistance.

    Please refer to the berrow.

     

    If client replace to AM26LV32E, which is it better the external resistance keep-attached or remove?

    The background, client want to examine what happens to a theoretical output, by the difference of Va~Vb by external resister "attached or nothing". (Usually, short, termination)

    - Is it right in the idea that Va~Vb=XX~YY[V] guarantees "H" on each conditions?

    - When right, how is the value of XX and YY decided?

    Moreover, does the structure of internal FailSafe differ in AM26LV32 and AM26LV32E?

    (If the 3rd page of the datasheet is both compared, internal resistance differs)

    Best regards,

    Satoshi

  • Satoshi-san,

    Do points XX and YY refer to the external device pins?
    The AM26LV32E has a better fail safe that is missing the potential issue that the AM26LV32 has.
    The external 1k resistors can be present or not. It will work well both ways.



  • Dear Ron Michallick-san

    I appreciate the quick reply.
    "XX~YY" is the range of VA~VB, to the inside of a device.
     
    ・If connect external 1kΩ resister

     ⇒Internal and external total.


    ・If not connect external 1kΩ resister
     ⇒nternal only.

     

    Best regards,

    Satoshi

  • Satoshi-san,

    TI-Tina (free application) circuit attached. Does this help?

    AM26LV32E.TSC
  • Dear Don Michallick-san

    Thank you for many reply.

    "–0.2V < Va-b < 0.07V" is indeterminate or logic"H", which does it become?

    Since the Tina-TI file (no external register) got the other day will be about Va-Vb=60mv by OPEN, it is set to spec-NG.

    Please let me check.

    0310.AM26LV32E - autosave 14-06-16 16_34.TSC

    And, Is there any data of status according to the range of Va-b?

    Example)

    ・Va-b > 0.2V    ⇒Logic "H"

    ・0.07V < Va-b < 0.2V    ⇒Logic" H"

    ・-0.2V < Va-b < 0.07V    ⇒indeterminate

    ・Va-b < -0.2V    ⇒Logic "L"

    Is it right in the above-mentioned idea?

    Best regards,

    Satoshi

  • As for the content on which it questioned the other day, how about the situation?

    Please teach if there are specs and information for which the confirmation is necessary to answer.

    I will confirm it.

     

    Best regards,

    Satoshi

  • Satoshi-san,

    Reality is the best teacher. So I tested many AM26LV32E receiver channels. The data supports that a VID of -200mV is certainly low and 0mV is certainly high. Anything in between is indeterminate.