Other Parts Discussed in Thread: DS90CF384A
Hello,
Features say ds90cf384a supports VGA, SVGA, XGA and Dual Pixel SXGA.
Does this chip support WVGA (800x480) ? If not, which chip could I use ?
Regards, Pierre
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: DS90CF384A
Hello,
Features say ds90cf384a supports VGA, SVGA, XGA and Dual Pixel SXGA.
Does this chip support WVGA (800x480) ? If not, which chip could I use ?
Regards, Pierre
Hi Pierre,
Thanks for providing more detailed information in a separate message:
=======================
I work on Android build project with a WVGA screen NHD-5.0-800480TF-ATXL#-CTP.
I use DS90CF384A to translate LVDS to RGB. It seems to work but image is dirty quality. I took a photo of the screen. It displays jpg image on the left, and unvarying colors on the right. You could see on the left, blue and red pixels lines. I also see some blinking pixels.
Here is my display conf in Android :
lvds-channel@0 {
reg = <0>;
fsl,data-mapping = "spwg";
fsl,data-width = <24>;
crtc = "ipu1-di0";
primary;
status = "okay";
/* Capacitive Display */
/*Configuration Newhaven 5.0 */
display-timings{
native-mode = <&timing0c>;
timing0c: newhaven5 {
clock-frequency = <27600000>; //Also tried 36MHz with same result
hactive = <800>;
vactive = <480>;
hback-porch = <87>;
hfront-porch = <41>;
vback-porch = <29>;
vfront-porch = <16>;
hsync-len = <2>;
vsync-len = <3>;
hsync-active = <0>;
vsync-active = <0>;
de-active = <1>;
pixelclk-active = <1>;
};
};
Do I have bad synchronization between RGB lines ? How your experience could explain this behaviour ?
=======================
It may be possible that you are not quite using the right clock for the display requirements. The 27.6 MHz value we provided is an estimate of the type of pixel clock we anticipate if a 20% blanking period is assumed. From the datasheet, it looks like the pixel clock frequency (DCLK frequency) is around 30-50 MHz. Can you try with 30 MHz as well as match your programmed porch and pulse width values with what is the New Haven Display specs? It looks like your values are a little different:
Thanks,
Michael
Hello Michael,
Thanks for your support with Jamille. Before writing on TI forum, I tried 30 MHz to 45 MHz Dclk conf with same result as 27,6 MHz. If I use typical spec values, the active area is partially out of display screen.
Here is my last try conf. I set hsync-len=48 (typical value) and adjust hback-porch=41 & hfront-porch=87 to center active area. I also set 31 MHz DCLK to reach 60fps (30 MHz = 58 fps).
clock-frequency = <31000000>;
hactive = <800>;
vactive = <480>;
hback-porch = <41>;
hfront-porch = <87>;
vback-porch = <29>;
vfront-porch = <16>;
hsync-len = <48>;
vsync-len = <3>;
hsync-active = <0>;
vsync-active = <0>;
de-active = <1>;
pixelclk-active = <1>;
I took a photo of the screen. It displays jpg image on the left, and unvarying colors on the right. You could see on the left, blue and red pixels lines. I also see some blinking pixels.
I will welcome any investigation ideas.
Best regards, Pierre