Hello, I would like to use the DP83620 and PTP for a physical layer application only (No MAC IP layer stack). To use the SYNC Eth feature, does the DP83620 need to see certain IP1588 packets to achieve synchronization with a remote slave device? Or can the DP83620 sync up on its own?
I am referencing SNLA100A (AN-1730), page 4, paragraph 3. "When SYNCE mode is enabled, control of the PTP clock, digital counter, and PTP rate adjust logic is switched to the recovered receive clock. This has the effect of locking the PTP clock and counter of the slave system to the PTP clock and counter of the master system."
I also notice that the DP83620 does not provide the PTP 1588 BASE REGISTERS like the DP83640 does.
In my application I am just using the Ethernet Physical layer (no IP stack). ideally I would like to have SYNCe automatically sync the master to slave without having to implement the 1588 protocol. It looks like the DP83620 is what I am looking for.
Regards,
Bob Ledoux
Edgetech