This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[DP83867IR] RGMII 1.8V connection

Other Parts Discussed in Thread: DP83867IR

Hi,

My customer wants to connection DP83867IR with AM335x using RGMII interface. Also, they want to use it by 1.8V VDDIO.
I are looking at "Electrical Characteristics" of both device's datasheet to check these connection.
In summary,
AM335x                   DP83867IR
VOH:1.35V(min)  =>  VIH 1.26V(min)
VOL:0.45V(max)  =>  VIL 0.35V(max)  ###"VOL > VIL"  NG!!!
VIH:1.17V(min)  <=  VOH 1.26V(min)
VIL:0.45V(max)  <=  VOL 0.35V(max)
[VDDIO=1.8V]
So, in case of 1.8V VDDIO, DP83867IR can NOT connect with AM335x.
Is my understanding correct?

Best Regards,
Taka