Part Number: DS90UB953-Q1
Other Parts Discussed in Thread: DS90UB954-Q1,
Hello,
we designed a system that transfers sensor data via fpd link using serializer/deserializer pair DS90UB953/DS90UB954.
The chips are connected via STP cable and we want to use the full bandwith transferring full HD at 60fps.
The IDX configuration of the serializer is set by hardware to IDX1 (I2C 8-Bit Address 0x30). I guess this is the COAX mode, as the system comes up with this mode after power up. Although we use an STP cable, the communication is working without errors at 30fps (half bandwith).
When we try to set the mode of both serializer and deserializer to STP (via I2C, the serializer first), the transmission looses look and there is no FPD3_CLK detected (see register settings below).
Is it possible to switch the cable mode in a running system? How can we set the IDX configuration to STP mode, there is no indication in the serializer datasheet (Table 8, page 21)?
Thanks and best regards,
Rolf