Part Number: DS90UB954-Q1
Other Parts Discussed in Thread: DS90UB953-Q1EVM,
I am asking the following questions for one of my customers:
I have been using the DS90UB954-Q1EVM and DS90UB953-Q1EVM boards to evaluate several coax cables.
1. The datasheets for the FPD III parts is very vague as to what the required attenuation budget is. Do you have any graphs that show the allowable attenuation vs frequency for this link? (such as a minimum S21 magnitude vs frequency plot)
2. What is the actual bandwidth requirements of the FPD III link? In the DS90UB953 datasheet, there is a paragraph in section 8.1 that outlines the forward channel. The frequencies called out do not make sense, since the only eye diagram listed in the datasheet shows that the edge transition time of the forward channel is 65ps, which would lead me to believe that 15GHz is the critical frequency. Is there more detailed information available on what the critical link frequencies are?
See Section 8.1 'Application Information' (DS90UB954 datasheet) and the eye diagram from section 6.8, figure 3.
3. I have been using TI's Analog LaunchPad tool with the DS90UB954-Q1EVM evaluation board. In the scripting folder for the 954, there is a script for doing link margin analysis (C:\Program Files (x86)\Texas Instruments\Analog LaunchPAD v1.57.0010\PreDefScripts\DS90UB954\ub954_margin_analysis_script). This script appears to be sweeping several link parameters to determine if a link can be maintained, and it produces a CSV file with the results. My question is, what is the parameters that it is sweeping? The columns are labeled as "SP" and the rows as "EQ", and I no mention of what the contents of the cells mean (I thought it was a 0 or a 1 for fail / pass, but I have seen a 0.3 appear once).
4. Related to question 3, how do I interpret results from the margin analysis tool? As in, how does the margin analysis help me determine that my selected cable will have enough margin to work in the field? I have attached the results on one of my cables for reference.
molex_1000660054_ub954sfeq_test.xlsx
Thank you for your support.