Part Number: DP83867IR
Hi
DP83867IR datasheet says as below,
"Configuration of the Aligned mode or Shift mode is accomplished via the RGMII Control Register (RGMIICTL), address 0x0032.
In Shift mode, the clock skew can be adjusted using the RGMII Delay Control Register (RGMIIDCTL), address 0x0086."
The following my understanding is correct?
In Shift mode(RGMIICTL 0x0032[0:1) = 11b), the clock skew can be adjusted using the RGMIIDCTL(0x0086).
Also, In Aligned mode(RGMIICTL 0x0032[0:1] = 00b), the RGMIIDCTL(0x0086) registers are disabled.
My customer try to check with Aligned mode. They could be adjusted using the RGMIIDCTL.
If my understanding is correct, please let me know the reason.
Muk