Part Number: ALP
Hi team,
#1 Could you please kindly help to see if there have something wrong when we use the Margin Analysis to do some test on ds90ub934. As the attached file shows, the test result is so ideal, and we think it is unreasonable. we have tried to setting different time like 5s,30s, it still show all green strops. If we do not select the "save result to file", it will have effect for the test result?
Test condition: cable length 1.6m, 913 connected with 934
#2 If we want to set the fixed EQ and SP value, like if i want to set EQ min to 6,EQ max to 9; Strop position min to 5, max to 10, could you please kindly help to provide some example code to set this value by indirect register configure way?
Thank you very much.