A related question is a question created from another question. When the related question is created, it will be automatically linked to the original question.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
SN75155: Hi, can you confirm if this connection SN75155 is correct?
No, V- is intended to connect to a power supply voltage of -4.5 V or lower in order to support RS-232 signaling, which is bipolar in nature. More modern transceiver devices implement a charge pump circuit in order to generate the higher-voltage, bipolar V+ and V- rails from a single logic rail (e.g., 5 V or 3.3 V); you may want to use one of those devices instead. You can find them here:
You can narrow down the search based on the number of TX and RX channels needed and other parameters like ESD immunity as required by your application.
If you have further questions on this please just let us know.