Part Number: DS90UB935-Q1
Hello, E2E members
Can you help to review the schematic and the register settings as attachment?
DS90UB935_934_936_Setting_20190603_r1p0a.pdf
Regards,
Nao
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB935-Q1
Hello, E2E members
Can you help to review the schematic and the register settings as attachment?
DS90UB935_934_936_Setting_20190603_r1p0a.pdf
Regards,
Nao
Hi Nao,
The block diagrams and register setting look good.
My only comment is that is DVP_CFG necessary (for 935/934)? What are you sending in DVP_DT_MAT_CH_VAL? If you are actually using that register, then this should be fine.
Best,
Jiashow
Hi Nao,
When you have reg 0x10[3] = b'1, the DVP block will allow packets with the DT from 0x11[5:0] (DVP_DT_MATCH_VAL) to go through regardless of the mode_75m or mode_100m setting. It doesn't seem like you are using it so you can simply set 0x10[3] = b'0.
Best,
Jiashow
Hi Nao,
My apology, I misread the register, please disregard what I said earlier about 0x10[3].
Setting 0x10[4] will allow any packets with DT to be pass through. If this is the intent it's fine.
Best,
Jiashow
Hello, Jiashow
Thnak you for your quick reply.
I forgot to check the one register setting too.
It are CLKOU_CTRLx.
I asked this register settings at other E2E.
https://e2e.ti.com/support/interface/f/138/t/800345
This register sets same vaule, isn't it?
0x06=0x41
0x07=0x0E
Regards,
Nao
Hi Nao,
For 935-934 RAW10 mode:
Line Rate = PCLK * 28 = 96 * 28 = 2.69Gbps
With reg 0x06 = 0x41 and 0x07 = 0x1C, you get a 24.0MHz CLKOUT
For 935-936 Sync mode:
Line Rate = 4G
If you want 24MHz clock, you need 0x06 = 0x43 and 0x07 = 0x7D.
If you want M/N integer, you can set to 23.8MHz clock by setting 0x06= 0x41 and 0x07 = 0x2A.
Best,
Jiashow