Part Number: DP83867IR
hi
1. In the evaluation,
A connection failure of 1000Base has occurred. Please tell me the possible cause and the your advice (register setting).
(Phenomenon)
When connecting to a 1000Base PC and auto negotiation,
PC side recognizes as 100Base
PHY side recognizes as 1000Base
The status become link up and the communication can not be performed.
(TEST condition)
Cable: Category 5e Cross 1m : the issue is 100% repeatable
>> No problem with 3m cable
>> Sometimes reproduced even with straight cable
>>There is no problem with Category 6 cable.
>>There is no problem with 1000base compliance test of LAN.
>>Customer think, Cable is no problem, because it was normal operation between PC and HUB by 1000base.
2. Could you please let me know the method of setting for limiting to only 100base/10base operation in the auto negotiation setting?
(In auto negotiation, only 1000base is excluded)
Muk