Part Number: TUSB321AI
Dear Sir:
In our system there are 2 power supply source, 1 is powered by USB, 2 is powered by POE.
In current system design, we use "CV_USB0_DETECT_VBUS” to detect USB insert or not.
If I powered by POE, the system could work. Theoretical "USB_5V(VDD Pin)” should be 0V, but there is slightly leakage due the system is powered on. Therefore, the value that I detect "USB_5V(VDD Pin)” is 0.376V, and the value "USB_C1(OUT2 Pin)” is 0.95V;
But according to Datasheet Page.4, OUT1 or OUT2 Max Voltage value is ”VDD + 0.3”.
In our case, 0.95V>0.376V+0.3V. Would it damage to ” TUSB321AI” ?