Part Number: TUSB9261
Hi,
I want to use the TUSB9261. USB to SATA bridge. in my design
The design Host use USB 2.0
it exist system the Host and the device are connected (board to board). the SATA device is removable.
Can I use USB 2.0 channel for programing the device? ( I read at the forms that someone had problems with that)
the Host using Linux as OS, Can you provide programing tool that supported Linux ?
Can you recommended SPI flash for use with the TUSB9261 (data sheet include obsolete parts)
can I program SPI flash diractly ? how?
Thanks in advance
Amir