Part Number: DP83867IR
Hi,
Our customer are using DP83867IR on their development board and
having an issue during IEEE 802.3 Ethernet Compliance test of 1000Base-T.
The test are failing at following section:
[1000 Base-T, Difference A,B Peak Output Voltage(w/ Disturbing Signal)]
[1000 Base-T, Point F Template Test(w/ Disturbing Signal)]
[1000 Base-T, Point H Template Test(w/ Disturbing Signal)]
Please take a look at attached file for the details.
Customer IEEE802.3 Ethernet Compliance Test Result.pdf
On the customer board, they are using RJ45 which magnetic's each center tap were
decoupled to the GND via 0.1uF independently.
And we check the schematics but it seem there no problem.
Also, we are following to the application report
"How to Configure DP838xx for Ethernet Compliance Testing",but it's failing.
We are searching for the cause of the failures, but we are stuck and no workaround are found yet.
What kind of problem can be considered against these test failure?
And what should we check to solve this test failure? Any advise will be helpful.
If possible, could you please check the customer's layout and schematics to find the issue?
This issue is similar to the following E2E thread.
e2e.ti.com/.../809921
In this thread, it was solved by updating the version of oscilloscope.
But we tested by using several different supplier's oscilloscope but it still fails.
So, it seems it's not oscilloscope problem.
best regards,
g.f.