Hello,
We have a desing of hub usb 3.0 with the TUSB8041.
A Few board works fine in USB 2.0 but doesn't work in 3.0.
The Other boards is working with 3.0 too.
Host controller(upstream side) is PCIe-USB converter chip.
And these interface is connected on the board(down Device).
So it is hard to trace the protocol.
Host chip recognized it is an entering compliance mode.
Is there some check point from experience?
A Host controller also has to be checked.
Can you help us?
Thank you